This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ds90ub949的DEMO搭配产品的928端,如何进行配置

如题,949的DEMO,我们产品是928,  匹配使用的话,步骤怎样的,如何进行配置?

  • 您好,
    首先确保硬件部分是没问题, strap pin引脚配置也都没问题,包括MODE引脚的配置等.
    2. 949端,配置IDx address。
    3. 928端,配置IDx address。 不知您host 接在928还是949端,和host 端接的为local device。
    4. 如果949 作为local device的话,enable 949的I2C pass through。
    5. 检查link detect 寄存器,确保link 没问题。
    6. 读取DES Device ID 寄存器(949的寄存器0X06)。