你好,我当前正在使用TLK2711A,速率为1.6Gbps(16bit,100Mhz),当使用10G SFP+ DAC铜缆(10Gtek,10GSFP+ Passive Copper CableAssembly)时,两端的2711收发正常,但是使用1.25G或者10G SFP+光模块(单模,1310nm)时异常,请问是什么原因,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我当前正在使用TLK2711A,速率为1.6Gbps(16bit,100Mhz),当使用10G SFP+ DAC铜缆(10Gtek,10GSFP+ Passive Copper CableAssembly)时,两端的2711收发正常,但是使用1.25G或者10G SFP+光模块(单模,1310nm)时异常,请问是什么原因,谢谢。
您好,根据您的描述,使用10G SFP+ DAC铜缆收发正常,但是使用10G SFP+光模块(单模,1310nm)异常,和您确认下,光模块是同一个光模块,但是线缆材质不同,导致的通信异常是吗?
光模块不同,10G SFP+ DAC铜缆使用的光模块是10Gtek 的 CAB-10GSFP-P1M:
Features
SFF-8431 Compliant
Broadband serial data rate operation:10 Mbps to 12 Gbps
Power Level I: 15 mW per cable end
100 Ohm differential impedance
Retractable pin latch
EEPROM signature
Pull to Release latch design
360°cable braid crimp
Enhanced EMI skirt design
Color options for strain relief and pull tab
Linear design for use with EDCs
AC-coupled inputs and outputs
30AWG to 24AWG cable available
Applications
10 Gigabit Ethernet and Gigabit
Ethernet (IEEE 802.3ae)
Fiber Channel: 1, 2, 4, 8, and 10GFC
Infiniband SDR, DDR, and QDR
Fiber Channel over Ethernet (FCoE)
Serial data transmission
而光模块是常用的普通1310nm、1550nm单模,使用光纤互连。10G SFP+光模块也测试了多个厂家,结果都不通。
您好,我们采用的光模块不兼容VML。另外,我们的开发板已经搭建好了,所以更改电路的方案可能不太有操作性。
而我们采用的能通信成功的DAC线缆是兼容Intel的,通信失败的10G光模块内部使用的是标准码,要是我们使用兼容Intel的码的光模块是否可行?