This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教THVD1451差分输入电压范围的问题

Other Parts Discussed in Thread: THVD1451

根据THVD1451的手册,该芯片供电电压VCC可以是3.3V~5V。

问题1,如果VCC是3.3V,差分输出管脚Y和Z的电压范围分别是0~3.3V;如果VCC是5,差分输出管脚Y和Z的电压范围分别是0~5V?这么理解对吧?

问题2,电脑端采用USB转422的接口芯片,差分输出电压范围为0~5V,将这个差分输出直接连接THVD1451的差分输入管脚A和B(THVD1451的VCC为3.3V),是否可以?是否损伤THVD1451? (A和B之间并联100欧姆电阻)

根据THVD1451手册,Absolute Maximum Ratings: input voltage范围是-0.3~5.7V. Recommended Operating Conditions: VI的范围是-15~15V。哪个是差分输入管脚的电压范围呢?

非常感谢!

  • 您好,
    1. driver的差分输出管脚Y和Z,或者receiver的差分输入管脚A和B,每个差分输入端的电压范围都是-15V~15V。 Vid=(A-B)或(Y-Z)的电压范围也是-15V~15V。
    2. 可以,0~5V在+-15V范围内,不会损伤THVD1451。
    3. Absolute Maximum Ratings中的-0.3V~5.7V的电压指的是控制引脚DE,RE和driver的输入引脚D的电压范围。 并且我们在使用芯片的时候,建议参考的是Recommend operating conditions中的电气参数,所以+-15V是差分输入电压的范围。
  • 非常感谢,十分受用!