Other Parts Discussed in Thread: THVD1451
根据THVD1451的手册,该芯片供电电压VCC可以是3.3V~5V。
问题1,如果VCC是3.3V,差分输出管脚Y和Z的电压范围分别是0~3.3V;如果VCC是5,差分输出管脚Y和Z的电压范围分别是0~5V?这么理解对吧?
问题2,电脑端采用USB转422的接口芯片,差分输出电压范围为0~5V,将这个差分输出直接连接THVD1451的差分输入管脚A和B(THVD1451的VCC为3.3V),是否可以?是否损伤THVD1451? (A和B之间并联100欧姆电阻)
根据THVD1451手册,Absolute Maximum Ratings: input voltage范围是-0.3~5.7V. Recommended Operating Conditions: VI的范围是-15~15V。哪个是差分输入管脚的电压范围呢?
非常感谢!