Other Parts Discussed in Thread: SN74AVC8T245, SN74LVC8T245
你好,
请问RGB接口应用电平转换,input VCCA=3.3V,output VCCB=1.8,分辨率1280*800 帧频60HZ,这两种SN74AVC8T和SN74LVC8T哪个能支持,还是两颗任意都可以选择,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74AVC8T245, SN74LVC8T245
你好,
请问RGB接口应用电平转换,input VCCA=3.3V,output VCCB=1.8,分辨率1280*800 帧频60HZ,这两种SN74AVC8T和SN74LVC8T哪个能支持,还是两颗任意都可以选择,谢谢~
您好1280*768@60Hz需要的时钟频率为79.5Mhz,那么1280*800@60Hz的像素时钟会更大一些。
SN74AVC8T245能支持的频率为320Mbps=160Mhz(VCCA ≥ 1.8 V and VCCB ≥ 1.8 V条件下)>80Mhz,所以可以支持。
SN74LVC8T245在VCCA=1.8V,VCCB=3.3V时,最大tpd=23.4ns,估算下来的data rate要比AVC系列的小很多。
所以二者相比,建议选择AVC系列。