亲爱的TI工程师,我现在需要把CPU输出的1.8V-CMOS 24MHz时钟信号分6路给摄像头使用。在TI首页选型结果是cdclvc1310和lmk00101,请问从应用合理性、成本和应用复杂度更推荐哪一款?或者还有更好的推荐吗?
我有看到CDCLVC1106PWR,但它输出是3.3V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
亲爱的TI工程师,我现在需要把CPU输出的1.8V-CMOS 24MHz时钟信号分6路给摄像头使用。在TI首页选型结果是cdclvc1310和lmk00101,请问从应用合理性、成本和应用复杂度更推荐哪一款?或者还有更好的推荐吗?
我有看到CDCLVC1106PWR,但它输出是3.3V。
LMK00101:第五页
CLKin0/0* and CLKin1/1* Input Clock Specifications, (5) (6)
PARAMETER TEST CONDITIONS MIN TYP MAX UNIT
VIH Input High Voltage * * Vdd V
VIL Input Low Voltage GND * * V
CDCLVC1310:第六页
Single-Ended DC Characteristic (PRI_INP, SEC_INP)(1)
PARAMETER TEST CONDITIONS MIN TYP MAX UNIT
VDD = 3.3 V ±5% 2 VDD + 0.3V V
VIH Input high voltage VDD = 2.5 V ±5% 1.6 VDD + 0.3 V V
VDD = 3.3 V ±5% –0.3 1.3 V
VIL Input low voltage VDD = 2.5 V ±5% –0.3 0.9 V