This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们在使用TXB0104做SPI总线电平转换时,出现小概率工作不稳定情况。
VCCA=1.8V,VCCB=3.3V
SPI的时钟速率为9.6MHZ,挂机12小时,有出现过5次通讯校验错误;
将SPI的时钟频率改为4.8MHZ后,挂机48小时,未出现异常。
请问:
1.是否有办法改善这个工作不稳定的办法?
2.如果无法改善,是不是TXB0104无法支持9.6MHZ的SPI通讯。