This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960 -Q1+ DS90UB935-Q1 链路不稳定问题

Other Parts Discussed in Thread: DS90UB960-Q1, DS90UB935-Q1

在我们的系统中,使用1个DS90UB960-Q1 连接4个camera 输入。
camera分辨率为1280x960@30fps, serializer是DS90UB935-Q1。
UB960提供同步信号给4个UB935, UB935以及camera的power均通过FPD-LINK提供。

在使用过程中,我们发现960与935之间的link存在不稳定的情况。
比如,上电并完成初始化以后,CPU端读UB960的寄存器,
会发现4个UB935中可能有1个,或者2个UB935对应的RX_PORT_STS1 Register (Address 0x4D),
其最低位LOCK_STS为0,表示“FPD-Link III receiver is NOT locked to incoming data”。
但是这个现象也不是每次上电后都会出现,有时4个link又都是LOCKED状态。

另外,即使最开始时4个link都是LOCKED状态,
但是在系统运行过程中,有时也会出现某个链路上的视频数据中断的情况。


会是什么原因导致以上不稳定现象呢?
可以帮助我们check一下原理设计以及PCB吗?