This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948寄存器配置没反应



您好,使用981双路FPD-LINK输入,948 OLDI输出;想要LVDS driver能力提升,按照数据手册给0X4B寄存器写入0X03,发现写入后LVDS Driver 并不会提高,测试眼图仍然显示的为默认值380mv,并不会上升到750mv,请问下除了0X4B需要配置,是否还需要配置其他的寄存器?第二个问题,在948进入PDB模式的时候,OLDI输出,一个通道电平为0V,一个通道电平为1V,请问为什么双路输出不同通道的电平表现的不一致?怎么去修改这个问题,使在PDB模式下,都为0V?

  • 您好,关于948 LVDS输出幅值的控制,需要先通过寄存器0x34[1:0]配置是port 0还是port 1 ,然后再配置0x4B,改变LVDS的幅值。
    另外, PDB 模式下,一个通道输出有1V的输出,这里应该是948锁存了一些随机的噪声信号,导致有1V输出。 参考948的上电时序,需要兼容的serializer 发送有效数据之后, 948 才启动,将PDB拉高,否则如果不满足这个条件的话,需要进行软件或硬件复位,防止948 锁存随机或噪声信号。 所以确认下948的上电时序是否满足datasheet中要求的。 参考Figure 9-1. Power Sequence。