This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ32000使用相关问题

1. 规格书中有提到The time keeping registers can take up to 1 second to update after the RTC switches from backup power supply to main power supply.,请问这句话的意思是当我从备用电源更改成VCC主要电源时,RTC计时的时间都会dealy?所以,当我多次来回更改备用电源和VCC主要电源时,RTC与真实的时间会越差越大?

2. 可以从pin IRQ去产生512Hz和1Hz的波形,请问产生的目的为何?

3. 目前crystal的Load capactiance是使用9pF,还有加上两颗15pF,请问这样的配置是否有问题?

翻譯結果

可以从pin IRQ去产生512Hz和1Hz的波形,请问产生的目的为何?
  • 您好,
    1、意思是当从备用电源切换为主要电源时,需要过1s才可以更新0-9寄存器的值
    2、做频率测试用
    2、数据手册推荐的Crystal load capacitance CL是12pF
  • Crystal load capacitance这个外加的电容,我认为需要考虑PCB板上走线的寄生电容,晶振自身的CL,使得最终为12pF±10%
  • 感谢Amy的回答。
    继续想询问,
    1. 经过这1s的转换会影响RTC的计时吗?RTC后续会delay吗?
    2. 如果使用不同的Crystal,可以从pin IRQ这边去调整频率是吗?
    3. 数据手册P5的Electrical Characteristics中提到,Backup supply voltage(Operating)的MIN电压为1.4V,Backup supply voltage(Switchover)的MIN电压为2.0V,请问这两者的差异是?
  • 1、电源切换不会影响RTC计时,只有当VCC > Vref时,寄存器才可以访问,并且当从备用电源切换为VCC电源后1s,主控端才可以访问或更新寄存器值;
    2、只可以外接32.768 kHz晶振
    3、Backup supply voltage(Operating)的MIN电压为1.4V是指没有VCC时,设备可以正常工作的Vback最小电压;
    Backup supply voltage(Switchover)的MIN电压为2.0V是指,当去掉VCC时,可以切换至备用电源的Vback电压;这里的意思是当Vback电压<2V时,去掉VCC电源,无法切换至Vback电源,设备将无法工作