This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI:
您好!我在芯片规格书中看到SN65C3238芯片最大可支持波特率到1Mbps,但是受工作电压和CL限制。
这里想和你们确认下这里的CL为哪些?
我这边使用的是1.8V的单品机+TXB0108PWR 3.3V电平转换+SN65C3238+PC,可以实现921600bps的要求吗?
另外TRSF3238E这款芯片的性能参数和SN65C3238有区别吗?
谢谢,期待你们的答复!
TXB0108能够支持的最大data rate为100Mbps,所以采用TXB0108进行1.8V~3.3V电平转换是没有问题的。
TRSF3238E和SN65C3238的主要区别在于TRSF3238E 包含了IEC61000-4-2 ESD防护等级,而SN65C3238没有。
所以这里的最大和最小,不知道如何理解。
另外针对探针的负载电容影响,不知道对于单片机和PC端的接口管脚电容会不会有影响。因为这边串口的波特率要求需支持921600bps。
这个需要实际验证下,921600bps的波特率应该没有问题,相比其他厂家的232产品,TI的232产品不论是在slew rate,supply current,output voltage, 以及功耗方面都占有一定的优势,另外,TI的232产品中像SN65C3243,SN75C3243,SN65C3238,SN75C3238的dara rate最高能达到1Mbps,其他的一般最高data rate在250Kbps。