This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

串行器和解串器的问题

Other Parts Discussed in Thread: DS90UH948-Q1, DS90UB953-Q1

您好:

请问一下,我们大概想这么使用,SENSOR---串行器---解串器----CPU,SENSOR输出是MIPI信号,解串器输出LVDS。

使用串行器DS90UB953-Q1和解串器ds90uh948-q1是否可行?

如果只是传输视频信号,不需要通过FPD-link传输I2C等控制信号,也不需要控制SENSOR,953和948是否自行串行和解串?还是需要进行配置?

如果953和948不可行,能否推荐满足要求的串行器和解串器?

  • 您好,95xx和93xx系列是不能兼容的,95x是属于ADAS系列的器件,93xx是属于IVI系列的器件,两者互不兼容。
  • 谢谢回复,再问一下,如果用953和954只传视频信号,其他的信号都不传,是不是使用953和954默认配置就可以了,还是说必须要对953和954配置视频才能串行和解串?

  • 您好, 默认配置应该也是可以工作的, 只是主机这边无法访问remote Des/Ser和remote slave, 视频信号还是可以进行传输的.
    因为比如953或954 都是支持内部pattern generation来进行BIST检测,看是否有图像发生,从而判断link是否没问题.
    所以不通过I2C传输控制信号的话,只通过serdes编解码,来传输视频信号我理解是可以的.