This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,我们采用8044A作为hub,downstream接了3个USB2.0的接口,upstream接了usb3.0/2.0,那么当数据传输的时候,upstream是走的usb 3.0的通道吗?数据速率上限是5Gb/s?谢谢
您好,TUSB8044A的上行端口的USB2.0和USB3.0的接口是分开的, 如果upstream port接了USB3.0和USB2.0的设备,那么3.0的速度是5Gbps,2.0 的是2.0 的高速速率.
此时下行端口是可以接任意速率的设备,各个port之间互不影响.
谢谢。那么当我upstream把3.0和2.0都接了,但下行端口接2.0设备,数据就走上行2.0的接口,当下行接了3.0设备,上行就走3.0的接口。我这么理解对吧。
您好,每个接口都是独立的,互不影响,只是说上行端口接了3.0和2.0的设备,那么下行接口也是可以接任意速度比如3.0或者2.0的设备,但是每个接口能够支持的速率都是独立的. 接3.0的设备支持的是3.0的速率,接2.0的是支持2.0的速率.
但是需要注意,如果上行端口接了只能支持高速,全速/低速的设备,那么下行端口就不能接3.0的设备了.
When the upstream port is connected to an electrical environment that only supports high-speed or full-speed/low-speed connections, SuperSpeed USB connectivity is disabled on the downstream ports.