Part Number: SN65DP159
SN65DP159 这颗芯片 TMDS 输出 为啥需要接 50R 上拉电阻,不接的话工作会不正常,没想明白原因

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好, 在datasheet中其实对输出需要上拉50ohm的原因有做介绍:The differential output driver provides a typical 10- mA current sink capability when no source term is enabled, which provides a typical 500-mV voltage drop across a 50-Ω termination resistor.
换句话说,TMDS和LVDS一样,是电流源模式逻辑架构, 在靠近DP159 端上拉50ohm的原因是为了拉电流创建一个AC电压,后面串联的100nF的AC耦合电容是隔直流,通交流的作用,目的就是允许DP159输出的交流信号输出到DP sink 端.