This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好, 3G HD/SD splitter, 推荐LMH0307, 它是1路输入,双路SDI输出的cable driver,请参考它的数据手册以及典型应用:
您好,感谢您的回复。
按照您的意思,我有几个问题需要再次与您确认下:
1,只需要使用LMH0307就可以实现1进2出的分路器 是吗?
2,GS2972输出信号,芯片内部是经过了SMPTE Cable Driver的,而LMH0307的输入是100Ω的差分,可以直接连接吗?
3,LMH0307可以直接按照下面的图片接入两个显示屏幕吗(使用75Ω同轴线缆)?
你好,我还想知道,我上面的方案是否也行了?
也就是LMH0324与lMH0397对接,输出两路SDI视频。
您好,LMH0397是无法实现1进2出的功能呢,请参考下它的内部架构:
您好,是的,看这个真值表您的理解是没问题的,CD mode下,LMH0397可以作为1:2 fanout的buffer器件,注意两路cable driver输出都是75ohm cable driver。