This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: DS90UB941搭配DS90UB948 接1920x720p屏显示暗红条纹如附件图片所示。

Part Number: DS90UB941AS-Q1


1. SOC端给941只送MIPI-CLK, DTA0信号全部不给数据。当941与948 link上时,就会出现如图片所示的异常暗红条纹。

2. SOC到941再到948的整个通路都是通的,可以显示SOC输出的画面,只是画面的底部也会叠加异常的暗红条纹。

3. 请教一下,该现象可能原因,需要重点检查哪一块电路?

  • 您好,根据您的描述,不给输入,只提供时钟信号,是想941内部产生的pattern传输给948,在显示面板上显示得到的图像是吗?如果使用的internal pattern 特性的话, 应该是配置的问题导致,那么寄存器0x64的pattern 类型您这边配置什么?默认的是显示黑白条,您看下0x64 bit[7:4]配置的是什么类型的输出? 

    另外,这是一篇关于Exploring the Int Test Pattern Generation Feature of FPDLink III IVI Devices的应用手册,里面给了几个参考示例,您可以参考下:

    www.ti.com/.../snla132g.pdf