Part Number: DS90UB964-Q1
Hi
请教下DS90UB964Q1是否支持和DS90UB953Q1配对?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要考虑带宽,964支持分辨率为720p/800p/960p@30/60Hz帧频。
Supports 1-Megapixel Sensors With HD 720p/800p/960p Resolution at 30-Hz or 60-Hz Frame Rate。
如果是200万像素,1920*1080@60Hz的分辨率,应该是不支持的,1080p@30hz是没问题的,因为964兼容933, 933的最大像素时钟为100Mhz,所以1080p@30hz可以,60hz应该是不支持的。
您好,您说的1920*1080*60hz 是camera的分辨率吧? 这个是要看serializer 是否支持,而964中的each lane 1.6Gbps指的是输出CSI的lane rate。
另外,分辨率的计算和数据格式没有关系,和color depth或者多少bit data有关系,比如RGB18bit或者YUV422 8bit的data。以24bit为例,
总的data rate计算Total data rate = [# active horizontal pixels + horizontal blanking] x [# active vertical lines + vertical blanking] x [frame rate] x [# bits/pixel]
那么each lane的lane rate=total data rate/lanes
比如964和953搭配使用,953 支持的是each lane为832Mbps的lane rate,我们可以通过上述公式计算下,以24bit为例,
total data rate=1920*1080*60*24=2.986Gbps,这里是没有将blanking计算在内,而953的能够支持的total data rate为3.328Gbps。
如果将blanking计算在内的话,应1080p@60hz,24bit total data rate应该是超过3.328Gbps的。