This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我打算使用TUSB8042A作为板载的USB HUB扩展USB使用(ARM64架构CPU LINUX系统),其中2个下游端口使用的是标准USB 插座,连接其他设备(U盘,鼠标、键盘等),其中2个端口在板子上直接使用,一个用于扩展WIFI,另一个用于扩展5G 网络,USB插座使用的2个端口打算使用负载开关,另外2个不使用电源管理功能,请问FULLPWRMGMTZ,PWRCTL1-4, OVERCUR1-4该怎么配置?
您好,不使用电源管理功能的话,FULLPWRMGMTZ可直接悬空。
同样,PWRCTL1-4内部已经集成下拉,并且为low时,不支持电池充电功能,所以可直接悬空。
OVERCUR1-4内部已经集成上拉,如果不使用,同样也可以直接悬空。