Part Number: SN65DSI86
SN65DSI86驱动屏,发现帧率只能到49Hz,请问如何才能让帧频率达到60Hz? clock 最大只能支持486Mhz,还能通过其他更改吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,DSI86的时钟最大486Mhz是没法修改的。
时钟决定了分辨率和帧率,如果提高帧率,可以降低分辨率。
目前49hz的帧率,分辨率是多少?
您的意思是DSI接收端的分辨率就是1920X1080@49Hz的是吗?但是eDP输出端需要输出60Hz的帧率才能点亮屏,是这个意思吗?
可以读取寄存器0xF6和0XF7是否有error,这两个寄存器发生error说明DSI86的配置和接收到DSI video的时序是不匹配的.其中DSI86的0x20 ~ 0x3A的这几个寄存器的配置很重要,这里有一篇关于DSI86的register configuration的FAQ,可以参考下:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/945404/faq-sn65dsi86-how-do-i-programming-the-sn65dsi86-registers