This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN24415-Q1

我在使用TLIN24415-Q1  时候MCU与TLIN24415-Q1进行SPI通讯时候出现无法通讯,en脚开始为低电平,mcu进行与TLIN24415-Q1通讯初始化时候将en脚拉高,当我读取TLIN24415-Q1设备id时候我先将cs脚拉低,发现读出来的数据为0,我在操作写的时候直接出现错误,请问是什么原因,另外有没有对TLIN24415-Q1进行配置的代码?或者具体配置TLIN24415-Q1寄存器的建议配置信息,谢谢!

  • 这个SPI 通讯出现我读TLIN24415-Q1设备的ID时候出现错误,例外怎么配置里面的TLIN24415-Q1寄存器,有没有例程或者 程序代码供参考,谢谢!

  • 您好,

    看下面datasheet中pin定义截图,3脚EN/nINT和9脚PIN/nCS 都是多功能管脚,取决于上电时PIN/nCS的电平状态,上电时如果PIN/nCS是低电平,TLIN2441工作在Pin Mode下;如果PIN/nCS是高电平或高阻态,工作在SPI模式下,为CS片选管脚。

    如果在Pin Mode下,EN/nINT就是使能EN功能;SPI模式下,EN/nINT管脚就是中断nINT功能。

    所以需要先确定上电时PIN/nCS的电平状态是什么