This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: 使用展讯平台T610 驱动京东方屏问题

Part Number: SN65DSI86


使用展讯T610主控,MIPI接口,驱动京东方1920X1080 @60HZ屏,发现帧率在49Hz可以正常刷新,将帧频率调试到60Hz(使用DSI TUNER配置寄存器), 无法正常显示了。

请问有展讯和MTK 驱动1920X1080 @60HZ以上的成功案例吗?

  • 您好,您的这个问题和E2E上的这个帖子类似,49fps的帧率可以正常显示,但是60fps的时候黑屏,您看参考下这个帖子:

    e2e.ti.com/.../sn65dsi86-the-display-screen-is-completely-black-when-the-resolution-is-3840-1080-60-fps-in-dual-dsi-to-dp-mode