你好,我这边采集的是NTC温度信号如图,电压VCC为5V,MOS打开后测量10路NTC两端电压,我要用ADC来做测量,请具体一点告诉我ADC输入应该配置那几个寄存器,应该怎么使用,我尝试了几次都没有成功,请以具体实例告之,我尝试了一周没有成功,不知道问题出在那里,请帮忙解答,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我这边采集的是NTC温度信号如图,电压VCC为5V,MOS打开后测量10路NTC两端电压,我要用ADC来做测量,请具体一点告诉我ADC输入应该配置那几个寄存器,应该怎么使用,我尝试了几次都没有成功,请以具体实例告之,我尝试了一周没有成功,不知道问题出在那里,请帮忙解答,谢谢
您好,
TIC12400-Q1主要是用来开关检测的,下面文档使用两个示例介绍了 配置 TIC12400-Q1 的过程:
https://www.ti.com.cn/cn/lit/pdf/scpa056
您的意思是您仅是要测TR1、RT2......RT10上的电压吗?
您好,TIC12400-Q1是一个多开关检测接口IC,我仔细看了下TIC12400-Q1datasheet,它应该是不能实现模拟电压的AD转换,它只能用来检测开关(数字开关或电阻编码开关)的状态,因此,建议您选用一个专用的ADC芯片实现您的电压检测应用
TIC12400-Q1是用来做开关检测的,它有一个wetting current会流经开关,当TRIGGER bit置1的时候,这个wetting current就会被激活,激活的话,会影响外接模拟电压检测的,因此在采集模拟电压时是不能被激活的。这个wetting current是可以通过WC_CFG0 Register设置为0的(默认值不需要配置),之前有个客户反馈说这个wetting current不能设置为0mA,后续他也没有给反馈,不知道最后是否解决了。目前,关于TIC12400-Q1的所有应用手册都是关于开关检测的,因此没有建议文档手册推荐给您。同时也不清楚您为什么选择这个多开关检测接口IC用于您的模拟电压采集