This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我采用的TFP410-EP芯片,接口类型是DVI显示接口,线缆是DVI-D,接DVI显示器发现:在1024X768分辨率下可以显示,1080P@60Hz,不能显示(显示器支持1080P分辨率);
把线缆换成DVI转HDMI,发现显示输出正常。且显示分辨率可达1080P;
我另外一个项目上使用的是TFP410芯片,接口也采用的DVI显示接口,采用DVI-D线缆接上述显示器,显示功能正常;分辨率可达1080P@60Hz。
请问TFP410和TFP410-EP除温度外还有什么区别吗?
您好,主要还是温度差异,我看了下TFP410-EP的像素时钟频率能达到165 MHz,1080p的像素时钟需要148.5MHz,所以EP系列支持1080p应该也是没问题的。
所以如果使用同一根线缆,同一个显示器的话,EP不能显示的话,应该是芯片问题,是否有更换一片试试呢?
换了一颗芯片还是不行,感觉这个状态像是在临界,无法排除是DVI链路问题还是TFP410输入的DVO信号的问题。。
TFP410-EP和TFP410的输入源不一样吗? TFP410-EP的输入IDCK频率是多少?
建议使用同样的测试条件,比如输入源相同,线缆相同,对比EP和TFP410的差异,这两款主要差异就是温度范围,电气性能都是一样的.
另外,您这里提到EP的话,DVI-D线缆更换成HDMI便能显示, 但TFP410或者TFP410-EP传输的TMDS信号,即使使用HDMI线缆,也是不包含音频信号的.
我在同一计算机板上:对比TFP410和TFP410-EP的测试效果一致。我更换开发板测试(开发板的DVI转换芯片不是TI的)发现有同样的问题,目前怀疑是前端输入的DVO信号匹配上有点问题。我这边想通过I2C接口调整TFP410芯片内部前端的控制信号的采样来尝试能否解决此问题。
好的, 测试中如果有任何关于TFP410或者EP的问题, 可再联系.