Hi 您好,
最近做项目,选择了TPS25750D,想通过I2Cs port配置SINK, UFP, 15V/3A output。有一些问题能否帮忙解答指点。
- datasheet此处是I2Cm吗?
The host should only use I2Cs_SCL/SDA for loading a patch bundle. Once the boot process is complete, the
port has a unique slave address on the I2Cm_SCL/SDA bus as selected by the ADCINx pins.

- 配置的这些decode值是指什么?

-我想配置TPS35750D为SINK, UFP, 15V/3A, 应该配置哪些寄存器?
我也在看技术手册,但是内容和寄存器比较多,能否给指点一下?
谢谢!