This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我遇到一个问题长期无法解决 写请示一下各位高手们
错误的讯息如下
===================================================================
[IPU1-0] 39.111877 s: src/bsp_deviceI2c.c @ Line 409:
[IPU1-0] 39.111968 s: Nrtos I2C3: DEV 0x3d: RD 0xf5 ... ERROR !!!
[IPU1-0] 39.112060 s: src/bsp_deviceI2c.c @ Line 466:
[IPU1-0] 39.112212 s: src/bsp_deviceI2c.c @ Line 477:
[IPU1-0] 39.112304 s: I2C3: Error timeout 5007 ms!!!
[IPU1-0] 44.116452 s: i2cMdSubmitChan: i2c transfer Timeout IRQ not received
[IPU1-0] 44.118068 s: src/bsp_deviceI2c.c @ Line 645:
[IPU1-0] 44.118190 s: I2C3: DEV 0x3d: WR 0x01 = 0x03 ... ERROR !!!
[IPU1-0] 44.118282 s: src/bsp_deviceI2c.c @ Line 667:
[IPU1-0] 44.118343 s: I2C3: Error timeout 5006 ms!!!
[IPU1-0] 44.118434 s: src/bsputils_ub960.c @ Line 1320:
[IPU1-0] 44.118495 s: Could not configure UB960 !!!
=======================================================
这是不是意味着我的ub962跟板子(I2c)无法沟通?
该如何解决这个问题
有哪些地方需要设定呢??
我有设置pinmux了
THANKS!!
您好,您指的I2C pass through enable吗?寄存器0x58 bit[7:6] enable I2C pass through和I2C pass through all 功能。
您好,I2C 总线timeout的原因是因为SCL保持长时间的low电平,导致会触发一个中断,所以发生这个报错,我认为可能需要检查下slave是否处于hang up挂起状态。 您参考下这篇应用手册32.3.7.3部分关于I2C SCL timeout的描述:https://www.ti.com.cn/cn/lit/ug/slau367p/slau367p.pdf
您好, 如果分析U962的I2C的话,我这边可能先用示波器测一下I2C的时序,然后如果发现SCL保持长时间的低电平,可能需要做一下复位看是否能解决. 我看您在英文E2E上也发帖咨询了,暂时还没得到回复,我这边帮您再push一下.