两个差分输入之间的R3是100欧姆,不给差分输入时,1A和1B无论是悬空还是通过50欧姆接地,1Y的输出都为高电平3.3V
此时测量1A和1B对地都为0V,1A和1B之间的电压也为0V,3.3V通过50欧姆接G,/G接地,其余3路引脚都是悬空的
为什么此时1Y的输出会是高电平呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两个差分输入之间的R3是100欧姆,不给差分输入时,1A和1B无论是悬空还是通过50欧姆接地,1Y的输出都为高电平3.3V
此时测量1A和1B对地都为0V,1A和1B之间的电压也为0V,3.3V通过50欧姆接G,/G接地,其余3路引脚都是悬空的
为什么此时1Y的输出会是高电平呢
您好,那是因为AM26LV32内部集成了失效保护电路,当输入端开路,短路或者终端连接的时候,输出都是一个有效的逻辑高状态。

谢谢,但是当我把1A和1B同时用50欧姆电阻下拉接地的时候,属于open,shorted或者terminated其中一种吗,这种情况下,输出也是3.3V
属于terminated,A和B同时接50ohm到地,相当于AB之间接了100ohm终端匹配电阻。所以此时输出应为high。
谢谢,那请问怎样才能保证输入不加的时候,输出是低电平呢,这个上电就是高电平不符合我们的需求
那可以考虑将receiver端的使能控制引脚G接低电平,G/接高电平,还是参考上述真值表,这样上电输出高阻态,但不是低电平。
然后需要总线有效的时候,再将G接高电平,同时G/为低电平。 可以使用GPIO来控制G的高低电平。