Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: DS90UB949-Q1
Hello TI:
1.我们使用贵公司的DS90UB948芯片,系统方案如下图,当FPD-LINK连接器短路或者断路的情况下,UB948芯片是否可以检测到?通过什么方法检测?
We use your company's DS90UB948 chip. The system scheme is as shown in the figure below. When the FPD-LINK connector is short-circuited or open, can the UB948 chip be detected? What methods are used to detect?
2.若检测到,是否可以通过某个GPIO(例如GPIO6)发送一个高电平给CPU?
If it is detected, can a high level be sent to the CPU through a certain GPIO (such as GPIO6)?