This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI guys,
we will use DS90UB927 communicate with DS90UB940,this case can be achived?and waht issue we need note?
how to config DS90UB927 this pad
Hello,first,the DS90UB940-Q1 is also backward-compatible with the DS90UB925Q-Q1, DS90UB925AQ-Q1, and DS90UB927Q-Q1 for PCLK frequencies ranging from 25 MHz to 85 MHz. Backward compatibility does not need to be enabled. When paired with a backward-compatible device, the deserializer auto-detects to 1-lane FPD-LinkIII on the primary channel (RIN0±).
As to the BKWD pin of DS90UB927, because 927 didn't need to be back compatible, it should be configured BKWD=0.
If BKWD=1 it means that 927 interfaces with 906/916.