This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rokin,
您好,都是可以的。
请问您在使用SN65lvcp408时是仅使用一种输入输出配对方式,还是使用trig模式,在两种输入输出配对方式之间切换?
如果是前者,根绝Datasheet P18 Table4和Table 5的说明,只有输出端口控制寄存器中Bit5-7决定输入输出配对关系;
如果是后者,根据Datasheet P18 Table4和Table 5的说明,输出端口控制寄存器中Bit5-7设置一种输入输出配对关系,输入端口控制寄存器Bit4-6设置另一种输入输出配对关系,然后通过写切换控制寄存器(Table 6)的标志位(Switch via I2C)或通过将SWT引脚置高,使得SN65lvcp408在两种配对关系间切换。