This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: 产品区别

Part Number: DS90UB913A-Q1

1.請問 DS90ub913 與 DS90ub933 差別

2.我想用 OV9716 (Sensor)+ OV492(ISP)+DS90ub913 

是否 DS90ub913 可傳輸到 1280*720P  60FPS

3.若 DS90ub913 不能 傳輸到 1280*720P  60FPS 是否可用 DS90ub933 或 DS90ub953

  • 您好,933和913 是pin to pin兼容的,二者的区别就在于12bit mode,933的像素时钟PCLK能达到100Mhz,而913在12bit mode PCLK最大为75Mhz。

    1280*720P  60FPS的话, 按照25%的blanking计算的话,计算得到PCLK的频率大概为70MHz左右,所以即使是12bit mode的话,也是能支持的,或者采用12bit ,100Mhz的933。

    10bit mode话,913的PCLK 能达到100Mhz,所以也是支持的。