This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: 关于如何配置949的寄存器进而访问948的寄存器的方法

Part Number: DS90UB949-Q1


你好,我想知道以下问题

949(mcu通过I2C控制949)目前已经连接到948了,也能检测到948的ID了

1.我想知道如何控制948的寄存器呢?是否是通过我的MCU输入948的I2C地址控制呢?

2.我想知道设置948的对应的IO口有哪些方法呢?

3.remote模式指的是949的那个寄存器的对应位呢?

Hello, I would like to know the following questions

949(MCU controls 949 via I2C) is now connected to 948 and can detect the ID of 948

1. I want to know how to control register 948.Is it possible to input 948's I2C address control through my MCU?

2. I would like to know how to set the IO port corresponding to 948?

3. Which bit of the register 949 does the remote mode refer to?