This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG720R-Q1: DP83TG720R-Q1上电后无法与外部设备进行通信,ping不通IP地址,但是led0-1都是亮着的,led_1一闪一闪,有发送字节,但是没有接收字节

Part Number: DP83TG720R-Q1


TI技术支持:

      您好!有个问题,DP83TG720R-Q1这个芯片与FPGA相连时,需要通过MDI和mdc对它进行初始化配置吗?还是说上电之后就可以正常工作?fpga是zu3eg。原理图参考EVM评估板设计的,做过两次板子,

第一次通过petalinux的ping 。。。。可以ping通fpga上的DP83TG720R-Q1,但是第二次就不行了,但是LED_1灯一闪一闪,一直闪,LED_0一直常亮状态,不知道是否正常,另外自己PING自己可以ping通。

谢谢技术支持,麻烦帮忙分析下!!