有4路mipi信号,想都通过953,然后再接到960,但4路mipi,分时,分不同lane接到953,这样可以实现吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,分时输入,应该是不可以的,因为对于输入信号来说,我们需要通过寄存器0x02配置好输入是2lane或者4lane或者1lane.

4个camera 数据的话,应该是采用4个UB953,然后deserializer 选择集成4路的Deserializer,我想您的应用是类似于下图中的应用: