This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962-Q1: 4 input not work

Part Number: DS90UB962-Q1



Dear TI engineer,

有个问题需要你帮忙
我们使用962 - 953,接了4颗AR0147(1.3Mp,1344x968x16bitx30fps)
单独点亮port0~port3都没有问题
点亮2颗或3颗147也没有问题
但在点亮四颗的时候,结果会是花屏

962 4lane
CSI_PLL_CTL 1.6Gbps
FPD3_MODE CSI-2 Mode

花屏时debug register 状态
register 0x47 = 0x0
register 0x54 = 0x0
register 0x35 = 0x3
register 0x52 = 0x0
register 0x5D = 0x20
register 0x5E = 0x20
register 0x5F = 0x20
register 0x60 = 0x20

Best regards,

Andy

  • 您好,您参考下英文E2E上的这个帖子,和您的问题类似,使用的camer型号也相同, 美国工程师给出的意见是可能在传输过程中信号发生反射,以及回波损耗或者插值损耗导致产生的噪声,建议是使用MAP tool来进行阈值分析,您参考下这个帖子中。

    e2e.ti.com/.../3800195