根据ONET4201LD的芯片手册描述,Vbias的调节范围为1V至3.5V,但是,芯片手册里没有介绍如何调节该电压值。
该芯片可以支持LDS-1310-DFB-2.5G-15/60-B-2-SM1-FA-CW-0.5(www.laser.com)吗?
该激光器的参数如下:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据ONET4201LD的芯片手册描述,Vbias的调节范围为1V至3.5V,但是,芯片手册里没有介绍如何调节该电压值。
该芯片可以支持LDS-1310-DFB-2.5G-15/60-B-2-SM1-FA-CW-0.5(www.laser.com)吗?
该激光器的参数如下:

您好,1~3.5V不是指的可调的,指的是激光二极管流入(sink)Bias端的偏置电流产生的偏置电压范围,在1V~3.5V范围都是正常的。
datasheet中给出Ibias的最大值不超过100mA。通过您给的激光器的参数,好像没有提供偏置电流的大小,其中的操作电流Iop可以和激光器的厂商确定一下,但是datasheet中给出了Ipd,即激光器的monitor sink电流,最大为5mA,附件中的激光器Im=5mA 是可以的,monitor diode的电压最大不超过1.6V。