This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK3131: 我是用FPGA与TLK313进行通信,发现只要复位结束,HSTL的接收端就一直在接收数据(

Part Number: TLK3131


您好,我是用FPGATLK313进行通信,发现只要复位结束,HSTL的接收端就一直在接收数据(发送端并没有发送任何数据),而且serdes的发送端与接收端也没有短接。之后,我将TLK3131的所有寄存器均在上电后读取了一遍(此时并没有任何配置,完全是默认状态)。发现以下几个寄存器的值与默认状态不符,不知是不是这个原因。

寄存器地址 手册中默认值 读取值

0x12 0x0000 0x4000

0x13 0x0000 0x8000

0x14 0x0000 0xC000

0X1C 0x0000 0x9000

0x1D 0xFFFD 0x0000

0x9013 0x0000 0x0004/0x0000

0x9014 0x0000 0x0004/0x0000

0x9200 0x0000 0x6300

0x9204 0x0000 0x1163

0x9205 0x0000 0xBB68

0x9206 0x0000 0x1102

0x9207 0x0000 0x100F

0x9208 0x0000 0x0100

硬件配置引脚配置如下:

serdes_sloop = 0; serdes_ploop = 0;

serdes_speed0 = 1; serdes_speed1 = 1;

serdes_code = 0; serdes_prbsen = 0; serdes_prtad = 5'b00000;

 

原理图添加在附件中,麻烦看一下是不是寄存器默认状态有问题导致的。

tlk3131_sch (1).pdf