This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: 设置成100M通信,会自动跳到10M通信上

Part Number: DP83848K


测试DP83848K 最先测试是OK, 放置一个月后再次测试,发现100M变成10M了,请问可能是什么原因造成。

  • 您好,您是采用的自动协商模式还是force 100Mbps mode?如果是自动协商的话,可以配置为force 100Mbps mode。

    速率从100M变成10M,有可能是提供时钟的晶振导致的,测量下晶振是否有很大的jitter,以及相位噪声很大?