This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,首先216的供电电压范围要宽为2.3V~6.5V。而211的供电电压范围为3V~3.6V,它是第一代USB redriver。
另外216内部集成了BC 1.2 CDP battery charging controller以及DC boost电路,而211没有。 相对于211,216的功能更多,redriver能力能强。
供电为3.3V。想使用216替代211,是否可行,电路上需要注意什么(看到了11脚的区别)
可行。总体性能216是优于211的。
11脚如果不用CDP battery charging 功能的话,高有效,可直接悬空, 因为内部已经上拉。