TI的工程师,你好,我在调试一个方案,TMDS IN ,HDMI OUT ,我更改DEC_FUNC_MODE为Automatic retimer for HDMI2.0时能出4K60,但是接显示器识别不了,接采集卡就能识别,显示器是能接受4K,560的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可能是和显示器阻抗不匹配导致,将TX_TERM_CTL引脚悬空,让其自动匹配终端电阻,看是否能显示?
采集卡能识别到,理论上来说DP159性能没问题。
您好,抱歉回复晚了。
TMDS_CLOCK_RATIO_STATUS 是否配置为1?采集卡能识别说明DP159的配置应该是没问题的。
显示器能识别到其他分辨率吗?如果能识别其他分辨率,那么在更改4K60的时候,读取下TMDS_CLOCK_RATIO_STATUS的值是否发生变化?
您好,您的意思是不需要配置的前提下,默认是否支持4K60是吗?
DEV_FUNC_MODE不更改的话,配置为01,01 - Automatic redriver to retimer crossover at 1.0 Gbps (default)
我理解的是,这时候是支持不到4K60的。4K60的话每个lane的data rate为6Gbps。