This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913Q-Q1: 使用OV10640连接DS90UB913Q,然后913和DS90UB960通过FPD-Link III连接,但是我不知道如何配置913A和960的初始化参数

Part Number: DS90UB913Q-Q1

ov10640输出的是12-bit RAW,1280*1080@60fps数据,DVP模式,针对于这种数据,如何配置DS90UB913Q的初始化参数

当前DS90UB913Q参数我是这样配置的:

0x03=0xC5
0x0D=0x99
0x14=0x02
0x05=0x2A
帮忙查看一下配置是否存在问题,如果存在问题请帮忙修正一下,谢谢