TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3122E: 串口乱码

Part Number: TRS3122E

上图为设计图纸。

环境描述:CPU的串口信号(1.8V)直接接到芯片上面然后转出接到连接器上面。C1/C2/C3选用的电容都是100nf/0402封装。C34/C35/C36也都是100nf、0402封装。V-约为-4.81V左右。

问题描述:TX/RX信号可以正常输出输入,但是输入输出均为乱码。请帮忙判断一下可能的原因、