This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下述日志是我配置dts以后 驱动输出的日志。
请问当前状态是否是正常状态?如果有问题是否能从下述日志获取出问题的原因?
谢谢!
[ 32.902263] TI DP83TC811 48485000.mdio:00: attached PHY driver [TI DP83TC811] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
[ 32.914188] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x4] data[0x20800001]
[ 32.921730] phy_read line:[722] reg:[0x4], data:[0x1]
[ 32.924135] 8021q: adding VLAN 0 to HW filter on device eth0
[ 32.928911] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x1] data[0x20200061]
[ 32.944777] phy_read line:[722] reg:[0x1], data:[0x61]
[ 32.951168] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x0] data[0x20002100]
[ 32.958635] phy_read line:[722] reg:[0x0], data:[0x2100]
[ 32.965200] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x0] data[0x20002100]
[ 32.972669] davinci_mdio_write line:[290] phy_id:[0x0] reg:[0x0] data[0x3300]
[ 33.998093] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x1] data[0x20200061]
[ 34.005569] phy_read line:[722] reg:[0x1], data:[0x61]
[ 34.010845] genphy_update_link line:[1530] link:[0]
[ 34.016646] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x5] data[0x20a00000]
[ 34.024082] phy_read line:[722] reg:[0x5], data:[0x0]
[ 34.030155] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x4] data[0x20800001]
[ 34.037615] phy_read line:[722] reg:[0x4], data:[0x1]
[ 35.118083] davinci_mdio_read line:[278] phy_id:[0x0] reg:[0x1] data[0x20200061]
[ 35.125523] phy_read line:[722] reg:[0x1], data:[0x61]
您好,看了下这个日志,应该是link 有问题,register 0x0001 = x61,如果link没问题的话正确的值应该为0x0065。
您好,单纯通过这个日志是不能判断是硬件问题还是软件配置问题。
或者您可以将您的配置或电路图附上以便分析,cable是否有链接? 是否和link partner有连接?
您好,R和C的值建议是按照datasheet中推荐的值。
另外,上述两个问题中,cable是否有和link partner连接?cable没问题吧?