由于中秋、国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSU6111A: 如何实现F280049C的UART转USB2.0到PC端的上位机

Part Number: TSU6111A

我使用的MCU的型号是280049C,我想实现MCU的UART转为USB2.0连通到PC端的上位机软件,想知道能否只使用TSU6111A就可以实现,

如果能实现是否需要对应的windows驱动,我目前的电路原理图如下

请问这样的原理图是否有错误?(目前使用的USB线缆无ID引脚,也尝试在芯片的ID引脚接上150K的电阻到地,PC都无法识别)

如果不能单独的使用280049C和TSU6111A芯片实现MCU的UART转USB到PC,请问是否需要有类似RS232或其他的芯片,如果有合适的能否推荐一下。

具体的连接方式是MCU-xxxx-TSU6111A-PC这种还是其他的连接方式?