This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: Single DSI -> 941AS -> Dual FPD -> 948 -> Display这个应用,是可以支持到1080p的,请问下具体配该如何实现?

Part Number: DS90UB941AS-Q1


 #1920x1080p60, Dual Link FPD III
# PCLK = 148.5MHz
# DSI clock = 445.5MHz
# DSI Lane Speed = 891Mbps/lane
# 4 Lanes DSI
# DSI input port 0
# DSI non-burst mode with sync pulses
# MODE_SEL0 strap = No. 3
# MODE_SEL1 strap = No. 0 or 1

具体寄存器:

{0x01,0x08}, //# Disable DSI

{0x40,0x04}, //# TSKIP_CNT
{0x41,0x05}, //# TSKIP_CNT
{0x42,0x30}, //# TSKIP_CNT

{0x40,0x10}, // # Init DSI Clock Settings (From Section 10.2 of datasheet)
{0x41,0x86}, //# Init DSI Clock Settings (From Section 10.2 of datasheet)
{0x42,0x0A}, // # Init DSI Clock Settings (From Section 10.2 of datasheet)
{0x41,0x94}, // # Init DSI Clock Settings (From Section 10.2 of datasheet)
{0x42,0x0A}, //# Init DSI Clock Settings (From Section 10.2 of datasheet)

{0x01,0x00}, //#Release DSI

实际读出0x5f=0x21 这样看的话 这个配置完全没有用呀  CLK都达不到