This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: USB to FIFO bridge 芯片

Part Number: TUSB9261


想咨询一下,TI公司有没有USB to FIFO bridge 芯片(转换成16bit或者32bit的并行总线),TUSB9261是这种芯片吗?

主要问题是,几乎找不到支持USB3.1(速率10Gbps,供电20V/5A),都是USB3.0(速率5Gbps,供电5V/0.9A),为什么呢?

谢谢

  • 您好,TUSB9261不能实现USB 转FIFO,它是一款USB转SATA的桥器件,SATA是串行型号。

    所以转并行总线这款不合适。

    我看了下,目前好像还没有USB转并行总线的桥器件,支持USB3.1的话目前也只有多路复用器可以支持到。