This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. TUSB4041和TUSB8041它们俩是通过I2C和SMBus接口和SOC进行通信么?参考电路中使用的是EEPROM,它是不需要上位机驱动么?
2. 如果作为I2C SLAVE与SOC进行通信它的器件地址是多少?
3.它内部的USB供电使能,是通过USB_D+/USB_D-来判断是否接入OTG设备?从而控制输出供电么?
您好,
1. 8041和4041是可以用SMbus接口和So通信的。4041和8041的的I2C EEPROM指的是4041/8041作为主机,去读取EEPROM中的内容。 配置为Smbus的话,4041/8041 作为从机,可以和主机进行通信。
2.如果作为从机,首先二者要配置SMBUSz=0 为SMbus模式,4041的从机地址为1000 1xyz;8041的从机地址也是1000 1xyz。xyz的具体配置为参考数据手册SMBus Slave Operation部分介绍。
3. 你指的USB Battery charging功能吗?关于USB 供电,我的建议是参考USB Battery Charging S pecification revision 1.2的协议中的具体描述。