Other Parts Discussed in Thread: THVD1400,
您好,我目前正在针对RS485芯片进行选型,目前在看THVD1406与THVD1400,两款芯片的第三管脚,一个是SHDN,一个是DE,问题如下:
1.针对1400这款芯片的DE和RE管脚,参考规格书图8-5,我理解的是,当MCU置低,发送器不使能,接收器使能,此时MCU接收并处理RXD信号,反之,当MCU置高,MCU接收并处理TXD信号。不知理解的对不对?
2.如果上条理解正确,那么针对1406芯片的SHDN与RE管脚,当芯片置低时,接收器使能,但同时也会激活关闭模式。按照规格书8.4章节描述,此时发送器和接收器都会关闭,那么此时RXD信号该如何传递至MCU中?
3.这两款芯片性能基本一致,那么1406和1400最大的不同应该就是第三管脚了,此外1406说的是“自动方向控制”,请问该怎么理解这个“自动方向控制”?
望回复,感谢。