DS125BR800 , 用这个芯片,现在测试10G网络,用的pin模式,然后发现有误码。能否请帮忙提供一下均衡芯片上跑10G网络,PIN模式的推荐配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS125BR800 , 用这个芯片,现在测试10G网络,用的pin模式,然后发现有误码。能否请帮忙提供一下均衡芯片上跑10G网络,PIN模式的推荐配置
您好,按照下面这个配置试试:
MODE: pull high(如用于8b10b测试,建议mode=0,如用于10G-KR 或者PCIe Gen3 应用,建议MODE=1)
RXDET: 如果3.3V供电,拉高至Vin,其他供电电压可以拉高到VDD.
开始的其他配置:
VOD =1000mV
DEM = 0 dB(DEM可以根据输出情况进行调节)
EQ 设置为最小。