This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1219: 12G-SDI 不能锁定

Part Number: LMH1219


1、首先在BNC接口用的是佳耐美的12G BNC端子;

2、PCB Layout遵守了高速走线的要求(75欧姆阻抗控制);

3、目前从BNC到LMH1219间的75欧姆PCB 走线长(包含中间的电容)在10mm,从LMH1219的差分输出到FPGA的PCB 走线长为65mm.

4、使用所有默认参数IN_OUT_SEL和OUT_CTRL 和VOD_DE管脚都是悬空的。

5、使用上述参数,可以稳定工作在6G模式,但12G输入后,FPGA一直会不能锁定信号,通过寄存器0x31,0x30调整不同的VOD和DEM,没有任何作用。

已经拿到了programming guide 的文档,但没有发现有意义的参考,请帮忙看看如何解决?