Part Number: DS90UB948-Q1
DS90UB948和947通讯,但是软件读到的948的I2C地址有时和硬件设置的IDX分压电阻不一样的值,测试分压电阻分的电压是对的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
DS90UB948和947通讯,但是软件读到的948的I2C地址有时和硬件设置的IDX分压电阻不一样的值,测试分压电阻分的电压是对的
我没找到948的下电时序要求,那应该是没有要求的。
您是对948 和 947 快速上下电吗?它们之前有初始化顺序:首先需要遵循数据表上的947 init序列,然后是init 948。
948也应该947开始发送有效的视频数据后通电。如果不满足此条件,则在接收到输入数据后,需要进行软件复位或硬复位(切换PDB引脚)。
SER先DES上电,是作为确保AEQ连接过程具有确定性的一种方法,您可以使用LOCK作为948已通电的指示器,建立初始锁定后,通过设置DES寄存器0x01=0x01或在DES处切换PDB,发出数字复位。除非由于电缆断开,SER/DES之间实际上没有连接,否则DES不会锁定。